Read-only |
About Balanced Measurements |
Description |
With a Single-ended - Single-ended - Balanced topology, returns the PNA port number that is connected to the Positive side of the DUT's Balanced Port. Use SetSSBPorts Method to set the port mapping for a Single-Ended - Single-Ended - Balanced topology. |
VB Syntax |
var = balTopology.SSB_BalPortPositive |
Variable |
(Type) - Description |
|
var |
(Long Integer) Variable to store the returned value. |
|
balTopology |
A BalancedTopology (object) |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
variable = balTopology.SSB_BalPortPositive 'Read |
C++ Syntax |
HRESULT get_SSB_BalPortPositive(long *bVal) |
Interface |
IBalancedTopology |