Write/Read
About Receiver Leveling

SafeMode Property


Description

Sets and returns the state of Safe Mode.

 VB Syntax

RxLevel.SafeMode(srcPort) = value

Variable

(Type) - Description

RxLevel

A ReceiverLeveling Object

value

(Boolean) Choose from:

True - Safe mode ON

False - Safe mode OFF

srcPort

(Long Integer) Source port for which to set the Safe Mode state for Receiver Leveling.

Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port

Return Type

Variant Boolean

Default

False

Examples

rxLevel.SafeMode (1) = True ' Write

value = rxLevel.SafeMode 2' Read

C++ Syntax

HRESULT get_SafeMode(long port, VARIANT_BOOL* pLevelingSafeMode);

HRESULT put_SafeMode(long port, VARIANT_BOOL LevelingSafeMode);

Interface

IReceiverLevelingConfiguration