Write/Read
About Safe Sweep

SafeSweepCoarsePowerAdjustment Property


Description

Set and read the Safe Sweep COARSE power adjustment.

 VB Syntax

gca.SafeSweepCoarsePowerAdjustment = value

Variable

(Type) - Description

gca

A GainCompression (object)

value

(Double)  Coarse power adjustment setting in dBm. Choose a value from +30 to (-30).

Return Type

Double

Default

3.0

Examples

gca.SafeSweepCoarsePowerAdjustment = 2.0 'Write

SSCourse = gca.SafeSweepCoarsePowerAdjustment 'Read

C++ Syntax

HRESULT get_SafeSweepCoarsePowerAdjustment(double* value)

HRESULT put_SafeSweepCoarsePowerAdjustment(double value)

Interface

IGainCompression