Write/Read
About Safe Sweep

SafeSweepFinePowerAdjustment Property


Description

Set and read the Safe Sweep FINE power adjustment.

 VB Syntax

gca.SafeSweepFinePowerAdjustment = value

Variable

(Type) - Description

gca

A GainCompression (object)

value

(Double)  Fine power adjustment setting in dBm. Choose a value from +30 to (-30).

Return Type

Double

Default

1.0

Examples

gca.SafeSweepFinePowerAdjustment = 0.1 'Write

SSfine = gca.SafeSweepFinePowerAdjustment 'Read

C++ Syntax

HRESULT get_SafeSweepFinePowerAdjustment(double* value)

HRESULT put_SafeSweepFinePowerAdjustment(double value)

Interface

IGainCompression