Write/Read
About Gain Compression

SaturationLevel Property


Description

Set and read the deviation dB from the maximum Pout. This is the point of saturation.

This value is used for Compression Method: Compression from Saturation.

 VB Syntax

gca.SaturationLevel = value

Variable

(Type) - Description

gca

A GainCompression (object)

value

(Double) - Saturation level in dB. Choose a value greater than 0.01 dB.

Return Type

Double

Default

.1 dB

Examples

gca.SaturationLevel = .5 'Write

satLevel = gca.SaturationLevel 'Read

C++ Syntax

HRESULT get_SaturationLevel(double* pVal)

HRESULT put_SaturationLevel(double newVal)

Interface

IGainCompression3