Write/Read. |
About Trigger |
Description |
Sets or returns the scope of a trigger signal. This determines whether a trigger signal affects a single channel or all channels in the PNA. Note: Trigger Modes Point and EverySweep require that Trigger.Scope be set to naChannelTrigger. |
VB Syntax |
trigsetup.Scope = value |
Variable |
(Type) - Description |
|
trigsetup |
A TriggerSetup (object) |
|
value |
(enum NATriggerType) - Trigger type. Choose from: 0 - naGlobalTrigger - a trigger signal is applied to all triggerable channels 1 - naChannelTrigger - a trigger signal is applied to the current channel. The next trigger signal will be applied to the next channel;not necessarily the next channel in numeric sequence (1-2-3-4 and so forth). |
Return Type |
Long Integer |
Default |
naGlobalTrigger |
Examples |
trigsetup.Scope = naGlobalTrigger 'Write |
|
trigtyp = trigsetup.Scope 'Read |
|
C++ Syntax |
HRESULT get_Scope(tagNATriggerType *pTrigger) |
Interface |
ITriggerSetup |