ShowKeysToolbarAtPowerOn Property

Write/Read
 

Description

This command controls the on/off state of the preference, "On Power-on show Keys toolbar".

 VB Syntax

pref.ShowKeysToolbarAtPowerOn = value

Variable

(Type) - Description

pref

A Preferences (object)

value

(Boolean) - Choose from:

True - Display the keys toolbar on power-on.

False - Do not display the keys toolbar on power-on.

Return Type

Boolean

Default

False

Examples

pref.ShowKeysToolbarAtPowerOn = True 'Write

value = pref.ShowKeysToolbarAtPowerOn 'Read

C++ Syntax

HRESULT get_ShowKeysToolbarAtPowerOn (VARIANT_BOOL* preference);

HRESULT put_ShowKeysToolbarAtPowerOn (VARIANT_BOOL val);

Interface

IPreferences16