Write/Read |
About E5091 Testset ControlAbout External Testset Control |
Description |
Turns ON and OFF the display of the test set control status bar. This status bar indicates the test set that is being controlled and the current port mappings. This setting is turned ON and OFF automatically when the test set is enabled or disabled. |
VB Syntax |
tset.ShowProperties = value |
Variable |
(Type) - Description |
|
tset |
A TestsetControl object. OR An E5091Testset object. |
|
value |
(Boolean) True - Turns display of testset properties ON. False - Turns display of testset properties OFF. |
Return Type |
Boolean |
Default |
False (True when test set control is enabled.) |
Examples |
|
C++ Syntax |
HRESULT get_ShowProperties(VARIANT_BOOL *state); |
Interface |
IE5091Testsets ITestsetControl |