Write-Read |
Description |
Specifies the behavior for guided cal steps that involve a sliding load in a cal that is about to be performed. Send this command BEFORE sending the Initialize command |
VB Syntax |
guided.SlidingLoadAcquisitionBehavior = value |
Variable |
(Type) - Description |
|
guided |
GuidedCalibration (object) |
|
value |
(Enum as NASlidingLoadAcquisitionBehavior) Choose from: 0 - naShowDialog - The ‘Move Sliding Load’ prompt is presented on the PNA screen. All slide positions are measured from a single invocation of the acquire command. 1 - naMeasureSlidePosition - Each invocation of the acquire command for a sliding load step measures a single slide position and increments the slide position counter. No ‘Move Sliding Load’ prompt is presented on the PNA screen. |
Return Type |
Enum |
Default |
0 – naShowDialog |
Examples |
obj.SlidingLoadAcquisitionBehavior = naMeasureSlidePosition |
C++ Syntax |
HRESULT put_SlidingLoadAcquisitionBehavior(enum NASlidingLoadAcquisitionBehavior behavior); HRESULT get_SlidingLoadAcquisitionBehavior(enum NASlidingLoadAcquisitionBehavior *behavior); |
Interface |
IGuidedCalibration10 |
Last Modified:
|
4-Dec-2012 |
New topic |