Write/Read
About Gain Compression

SmartSweepMaximumIterations Property


Description

Set and read the maximum permitted number of iterations which SMART Sweep may utilize to find the desired compression level, to within the specified tolerance.

 VB Syntax

gca.SmartSweepMaximumIterations = value

Variable

(Type) - Description

gca

A GainCompression (object)

value

(integer) - Maximum number of iterations. Choose a value between 1 and 50.

Return Type

Integer

Default

20

Examples

gca.SmartSweepMaximumIterations = 10 'Write

iters = gca.SmartSweepMaximumIterations 'Read

C++ Syntax

HRESULT get_SmartSweepMaximumIterations(int* pVal)

HRESULT put_SmartSweepMaximumIterations(int newVal)

Interface

IGainCompression