Write/Read |
Description |
Set and read the stop frequency value for a specific port. |
VB Syntax |
chan.SourcePortStopFrequency(port) = value |
Variable |
(Type) - Description |
chan |
A SA Channel (object) |
port |
(long) Source port number for which to set the stop frequency value. |
value |
(double) Stop frequency value. |
Return Type |
double |
Default |
1 |
Examples |
chan.SourcePortStopFrequency(1) = 1e9 'Write |
value = chan.SourcePortStopFrequency(1) 'Read |
|
C++ Syntax |
HRESULT put_SourcePortStopFrequency(long port, double value); HRESULT get_SourcePortStopFrequency(long port, double* value); |
Interface |
IChannel26 |