Write / Read |
About Source Power Cal |
Description |
Sets source power correction ON or OFF for a specific source port on this channel, or returns the current ON or OFF state of correction for that source port. |
VB Syntax |
chan.SourcePowerCorrection (srcPort) = value |
Variable |
(Type) - Description |
|
chan |
(object) – A Channel object |
|
srcPort |
(long integer) – Source port for which to set or return the ON or OFF state of source power correction. Note: If the port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-x model, then you must use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port. |
|
value |
(boolean) False – Turns source power correction OFF for the source port. True – Turns source power correction ON for the source port. |
Return Type |
Boolean |
Default |
False - Source power correction will turn correction ON |
Examples |
chan.SourcePowerCorrection(1) = False 'Write |
C++ Syntax |
HRESULT put_SourcePowerCorrection(VARIANT_BOOL bState); HRESULT get_SourcePowerCorrection(VARIANT_BOOL *bState); |
Interface |
IChannel |