Write/Read
About Source Power

SourcePowerOption Property


Description

Enables the source power to be set on individual sweep segments. This property must be set True before seg.TestPortPower = value is sent. Otherwise, the test port power command will be ignored.

 VB Syntax

segs.SourcePowerOption = state

Variable

(Type) - Description

segs

A Segments collection (object)

state

(boolean)

True - Enables variable TestPortPower to be set segment sweep

False - Disables variable TestPortPower to be set segment sweep

Return Type

Boolean

Default

False

Examples

segs.SourcePowerOption = True 'Write

powerOption = SourcePowerOption 'Read

C++ Syntax

HRESULT get_SourcePowerOption(VARIANT_BOOL *pVal)
HRESULT put_SourcePowerOption(VARIANT_BOOL newVal)

Interface

ISegments