Read-only

 

Span Property


Description

Returns the stimulus span of the measurement (stop-start data points). To understand how this property is useful, see IMeasurement2 Interface.

 VB Syntax

value = meas.Span

Variable

(Type) - Description

value

(Double) - Variable to store the returned value.

meas

A Measurement  (object)

Return Type

Double

Default

Not Applicable

Examples

Print meas.Span 'prints the span of the measurement

C++ Syntax

HRESULT get_Span(double * Val);

Interface

IMeasurement2