Write/Read

State Property


Description

Turns the specified pulse generator ON and OFF.

 VB Syntax

pulse.State (n) = value

Variable

(Type) - Description

pulse

A PulseGenerator (object)

n

(Integer) Pulse generator number. Choose from 0 to 4.

Or use PulseGeneratorID to refer to an external pulse generator.

0 is the generator that pulses the ADC.

value

True - turns pulse output ON.

False - turns pulse output OFF.

Return Type

Boolean

Default

False

Examples

pulse.State(1) = True 'Write

value = pulse.State(4) 'Read

C++ Syntax

HRESULT get_State(integer pulse, VARIANT_BOOL *pVal);

HRESULT put_State(integer pulse, VARIANT_BOOL newVal);

Interface

IPulseGenerator