Read-only |
About Cal sets |
Description |
Returns the stop frequency that is stored in the Cal Set. |
VB Syntax |
value = CalSet.StopFrequency (range) |
Variable |
(Type) - Description |
|
value |
(double) - returned Stop frequency in Hertz. |
|
CalSet |
CalSet (object) |
|
range |
(Long) Choose: 0 (Source and receiver frequency) |
Return Type |
Double |
Default |
Not Applicable |
Examples |
stop = calset.StopFrequency(0)'Reads the stop frequency stored in the cal set. |
C++ Syntax |
HRESULT get_StopFrequency(long range, double *pVal) |
Interface |
|CalSet3 |
Last modified:
|
25-Jan-2011 |
Fixed range argument |
|
Nov. 1, 2006 |
New command - split from ch.StopFreq |