Write/Read
About Modifying Cal Kits

TZReal Property


Description

Sets and Returns the TZReal value (the real Terminal Impedance value) for the calibration standard. Only applicable when "Type" is set to naArbitraryImpedance.

To set the other resistance values, use TZImag

 VB Syntax

calstd.TZReal = value

Variable

(Type) - Description

calstd

A CalStandard (object). Use calKit.GetCalStandard to get a handle to the standard.

value

(single) - Value for TZReal in Ohms

Return Type

Single

Default

Not Applicable

Examples

calstd.TZReal = 15 'Write the value of TZReal to 15 Ohms

imp0 = calstd.TZReal 'Read the value of TZReal

C++ Syntax

HRESULT get_TZReal(float *pVal);
HRESULT put_TZReal(float newVal);

Interface

ICalStandard2