Write/Read
About IM Spectrum Tracking

TrackingManualStepEnable Property


Description

Sets and returns the step sweep mode for the IM Spectrum channel.

 VB Syntax

ims.TrackingManualStepEnable = value

Variable

(Type) - Description

ims

An IMSpectrum Object

value

(Boolean) Choose from:

False - Automatic Step

True - Manual Step

Return Type

Boolean

Default

False - Automatic Step

Examples

ims.TrackingManualStepEnable = True 'Write

value = ims.TrackingManualStepEnable 'Read

C++ Syntax

HRESULT get_TrackingManualStepEnable(VARIANT BOOL *bVal)
HRESULT put_TrackingManualStepEnable(VARIANT BOOL newVal)

Interface

IIMSpectrum