Write/Read
About ExternalDevices

TriggerMode (ExtendedProperties) Property


Description

Sets and returns the trigger mode for an external source.

 VB Syntax

extSource.TriggerMode = value

Variable

(Type) - Description

extSource

An ExternalSource Object (object)

value

(enum NAExtDevTriggerMode) - Choose from:

0 - naExtDevTriggerModeCW

1 - naExtDevTriggerModeHW

Return Type

Enum

Default

0 - naExtDevTriggerModeCW

Examples

extSource.TriggerMode = naExtDevTriggerModeCW 'Write

tm = extSource.TriggerMode 'Read

C++ Syntax

HRESULT get_TriggerMode (tagNAExtDevTriggerMode *pMode)
HRESULT put_TriggerMode (tagNAExtDevTriggerMode newMode)

Interface

IExternalSource