Write/Read
About Auxiliary Triggering

TriggerOutDuration Property


Description

Specifies the width of the output pulse, which is the time that the Aux trigger output will be asserted.

 VB Syntax

auxTrig.TriggerOutDuration = value

Variable

(Type) - Description

auxTrig

An AuxTrigger (object)

value

(single) - Duration value in seconds. Choose a value between 1E-6 and 1.

Return Type

Double

Default

1E-6 sec

Exaamples

auxTrig.TriggerOutDuration = 1e-3 'Write

value = auxTrig.TriggerOutDuration 'Read the value

C++ Syntax

HRESULT get_TriggerOutDuration(double *val);
HRESULT put_TriggerOutDuration(double val);

Interface

IAuxTrigger