Write/Read. |
About Modifying Cal Kits |
Description |
Sets and Returns the type of calibration standard. |
VB Syntax |
calstd.Type = value |
Variable |
(Type) - Description |
calstd |
A CalStandard (object). Use calKit.GetCalStandard to get a handle to the standard. |
value |
(enum NACalStandardType) -Choose from: |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
calstd.Type = naOpen 'Write |
standardtype = calstd.Type 'Read |
|
C++ Syntax |
HRESULT get_Type(tagNACalStandardType *pVal) |
Interface |
ICalStandard |