Read-only |
About External Testset Control |
Description |
Returns the testset model number. |
VB Syntax |
tset.Type model |
Variable |
(Type) - Description |
model |
(String) Variable to return the Test set model |
tset |
A TestsetControl object. Obtained from the ExternalTestsets collection. |
Return Type |
String |
Default |
None |
Examples |
testset.type model |
C++ Syntax |
HRESULT get_Type(BSTR *pType); |
Interface |
ITestsetControl |