Read-only
 

UsedChannelNumbers Property


Description

Returns an array of channel numbers that are in use. A used channel has at least one measurement subscribed to it

VB Syntax

chanNumbers = chans.UsedChannelNumbers

Variable

(Type) - Description

chanNumbers

Variable array to store the returned channel numbers

chans

A Channel collection (object)

Return Type

One-dimensional array of long integers

Default

Not Applicable

Examples

chanNumbers = chans.UsedChannelNumbers

C++ Syntax

HRESULT get_UsedChannelNumbers(VARIANT* channelNumbers);

Interface

IChannels2