Read-only
About ECal User Characterization

UserName Property


Description

Sets and reads the description of the person and/or company who is producing the ECal user characterization. This description is stored with the characterization in the ECal module.

Set this description before sending Initialize or the default (empty string) will be used.

 VB Syntax

userChar.UserName = value

Variable

(Type) - Description

userChar

An ECalUserCharacterizer Object

value

(String) Descriptive text, limited to 19 characters maximum.

Return Type

String

Default

"" (Empty String)

Examples

userChar.UserName = "John Doe, Acme Inc."

C++ Syntax

HRESULT get_UserName(BSTR *name);

HRESULT put_UserName(BSTR name);

Interface

IECalUserCharacterizer