Write/Read |
About User Preset |
Description |
'Checks' and 'clears' the enable box on the User Preset dialog box. This only affects subsequent Presets from the front panel user interface. Regardless of the state of the User Preset Enable checkbox, the app.Preset command will always preset the PNA to the factory preset settings, and app.UserPreset will always perform a User Preset. |
VB Syntax |
app.UserPresetEnable = state |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
state |
(boolean) Front Panel User Preset State. Choose from: False – User Preset OFF True – User Preset ON |
Return Type |
Boolean |
Default |
False |
Examples |
app.UserPresetEnable = True 'Write |
|
upreset = app.UserPresetEnable 'Read |
|
C++ Syntax |
HRESULT get_UserPresetEnable(VARIANT_BOOL *pVal) |
Interface |
IApplication6 |