Write/Read

Visible Property


Description

Makes the Network Analyzer application visible or not visible. In the Not Visible state, the analyzer cycle time for making measurements can be significantly faster because the display does not process data.

 VB Syntax

app.Visible = state

Variable

(Type) - Description

app

An Application (object)

state

(boolean)

False - Network Analyzer application NOT visible

True - Network Analyzer application IS visible

Return Type

Boolean

Default

True

Examples

app.Visible = False 'Write

vis = app.Visible 'Read

C++ Syntax

HRESULT get_Visible(VARIANT_BOOL * bVisible)
HRESULT put_Visible(VARIANT_BOOL bVisible)

Interface

IApplication