Write/Read
About Scale

YScale Property


Description

Sets or returns the Y-axis Per-Division value of the active trace.

 VB Syntax

trace.YScale = value

Variable

(Type) - Description

trace

A Trace (object)

value

(double) - Scale /division number. Units and range depend on the current data format.

Return Type

Double

Default

10 (db)

Examples

trac.YScale = 5 'Write

yscl = trac.YScale 'Read

C++ Syntax

HRESULT get_YScale(double *pVal)
HRESULT put_YScale(double newVal)

Interface

ITrace