These commands are used to control the Automatic Fixture Removal (AFR) capabilities in the PNA.
AFR: FIXTure: | INPuts | PREView | DATA | REFZ SAVE: | FILename | PORTs | TYPE STANdard: | DATA | EDIT: | FLENgth | GATE | METHod | LOAD | THRU | USE
|
Click on a keyword to view the command details.
See Also
(Read-Write) This command selects whether the fixture is band limited or not. |
|
Parameters |
|
<bool> |
Band limited or not. Choose from: ON (or 1) - Band limited. OFF (or 0) - Not band limited. |
Examples |
AFR:FIXTure:BLIMited ON |
Query Syntax |
AFR:FIXTure:BLIMited? |
Return Type |
Boolean |
Default |
OFF |
(Read-Write) This command selects whether to use DUT correction or not when the characterization fixture is not equal to the DUT measurement fixture. |
|
Parameters |
|
<bool> |
DUT correction state. Choose from: ON (or 1) - Use DUT correction. OFF (or 0) - Do not use DUT correction. |
Examples |
AFR:FIXTure:CDUT ON |
Query Syntax |
AFR:FIXTure:CDUT? |
Return Type |
Boolean |
Default |
OFF |
(Read-Write) This command selects Fixture Length A not equal to B correction. |
|
Parameters |
|
<bool> |
Correction match state. Choose from: ON (or 1) - Correct. OFF (or 0) - Do not correct. |
Examples |
AFR:FIXTure:CLENgth ON |
Query Syntax |
AFR:FIXTure:CLENgth? |
Return Type |
Boolean |
Default |
ON |
(Read-Write) This command selects Fixture Match A not equal to B correction. |
|
Parameters |
|
<bool> |
Correction match state. Choose from: ON (or 1) - Correct. OFF (or 0) - Do not correct. |
Examples |
AFR:FIXTure:CMATch ON |
Query Syntax |
AFR:FIXTure:CMATch? |
Return Type |
Boolean |
Default |
ON |
(Read-Write) This command describes the fixture inputs (single ended or differential). |
|
Parameters |
|
<char> |
Choose from: SENDed - Single ended fixture inputs. DIFFerential - Differential fixture inputs. |
Examples |
AFR:FIXTure:INPuts SENDed |
Query Syntax |
AFR:FIXTure:INPuts? |
Return Type |
String |
Default |
SEND |
(Read-Write) This command selects the number of fixtures to be characterized. |
|
Parameters |
|
<num> |
Choose from 1, 2, or 4. |
Examples |
AFR:FIXTure:MEASurement 2 |
Query Syntax |
AFR:FIXTure:MEASurement? |
Return Type |
Numeric |
Default |
2 |
(Write-only) This command refreshes preview data. It is required that this command be sent before a query gate, fixture length, and impedance data. |
|
Parameters |
None |
Examples |
AFR:STANdard:EDIT:GATE
AFIX,0.485 |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
(Read-only) This command reads the impedance profile of the calculated fixture model. |
|
Parameters |
|
<char_param> |
Selected impedance term. Choose from: ASENded - Single-Ended ZA BSENded - Single-Ended ZB ADIFf - Differential ZA BDIFf - Differential ZB ACOMm - Common mode ZA BCOMm - Common mode ZB |
Examples |
AFR:FIXTure:PREView:DATA:IMPedance? ADIF |
Return Type |
Block Data |
Default |
Not Applicable |
(Read-only) This command reads the impedance profile of the calculated fixture model at a specified position. |
|
Parameters |
|
<char_param> |
Selected impedance term. Choose from: ASENded - Single-Ended ZA BSENded - Single-Ended ZB ADIFf - Differential ZA BDIFf - Differential ZB ACOMm - Common mode ZA BCOMm - Common mode ZB |
<num_x> |
The X-axis position (ns), where the Y-axis value will be returned. |
Examples |
AFR:FIXTure:PREView:DATA:IMPedance:MARKer:Y? ADIF,0.5 |
Return Type |
Numeric |
Default |
Not Applicable |
(Read-Write) This command chooses the calibration reference Z0 after fixture removal. |
|
Parameters |
|
<char> |
Choose from: SYSZ- System Z0. MEAZ - Measured fixture Z0. CUSTom - User input. |
<num> |
Optional argument. If <char> is set to CUST, this is the user input vale for Z0. |
Examples |
AFR:FIXTure:REFZ SYSZ AFR:FIXTure:REFZ CUST,52.0 |
Query Syntax |
AFR:FIXTure:REFZ? |
Return Type |
String (SYSZ, MEAZ, or CUST) |
Default |
SYSZ |
(Write-only) Restores the default AFR settings. |
|
Parameters |
None |
Examples |
AFR:INIT |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
(Read-Write) This command specifies the file paths of saved fixture data. |
|
Parameters |
|
<string> |
Fixture A path. |
<string> |
Fixture B path. |
Examples |
AFR:SAVE:FILename 'C:\fixA.s2p','C:\fixB.s2p' |
Query Syntax |
AFR:SAVE:FILename? |
Return Type |
String |
Default |
"C:\fixA.s2p,C:\fixB.s2p" |
(Read-Write) This command assigns the ports for saved fixture data in several formats. |
|
Parameters |
|
<char> |
Port assignment. Choose from: VNA - VNA format. ADS - ADS format. |
Examples |
AFR:SAVE:PORTs VNA |
Query Syntax |
AFR:SAVE:PORTs? |
Return Type |
String |
Default |
VNA |
(Read-Write) This command sets the file type to save fixture data. |
|
Parameters |
|
<char> |
Impedance method. Choose from: TSONe - Touchstone file type. TSTWo - Touchstone 2 file type. CITifile - Citifile file type. |
Examples |
AFR:SAVE:TYPE TSONe |
Query Syntax |
AFR:SAVE:TYPE? |
Return Type |
String |
Default |
TSONe |
(Read-Write) This command selects all OPEN standards. |
|
Parameters |
|
<bool> |
Select all OPEN standards or not. Choose from: ON (or 1) - Use all OPEN standards. OFF (or 0) - Do not use all OPEN standards. |
Examples |
AFR:STANdard:ALLOpen ON |
Query Syntax |
AFR:STANdard:ALLOpen? |
Return Type |
Boolean |
Default |
OFF |
(Read-Write) This command selects all SHORT standards. |
|
Parameters |
|
<bool> |
Select all SHORT standards or not. Choose from: ON (or 1) - Use all SHORT standards. OFF (or 0) - Do not use all SHORT standards. |
Examples |
AFR:STANdard:ALLShort ON |
Query Syntax |
AFR:STANdard:ALLShort? |
Return Type |
Boolean |
Default |
OFF |
(Read-only) This command reads the impedance profile of the measured standard. |
|
Parameters |
|
<char_std> |
Selected standard. Choose from: THRU - 2X Thru STHRu - Second 2X Thru FDUT - Fixtured DUT AOPen - Fixture A Open BOPen - Fixture B Open ASHort - Fixture A Short BSHort - Fixture B Short |
<char_param> |
Selected impedance term. Choose from: ASENded - Single-Ended ZA BSENded - Single-Ended ZB ADIFf - Differential ZA BDIFf - Differential ZB ACOMm - Common mode ZA BCOMm - Common mode ZB |
Examples |
AFR:STANdard:DATA:IMPedance? AOP,ADIF |
Return Type |
Block Data |
Default |
Not Applicable |
(Read-only) This command reads the impedance of the measured standard at a specified position. |
|
Parameters |
|
<char_std> |
Selected standard. Choose from: THRU - 2X Thru STHRu - Second 2X Thru FDUT - Fixtured DUT AOPen - Fixture A Open BOPen - Fixture B Open ASHort - Fixture A Short BSHort - Fixture B Short |
<char_param> |
Selected impedance term. Choose from: ASENded - Single-Ended ZA BSENded - Single-Ended ZB ADIFf - Differential ZA BDIFf - Differential ZB ACOMm - Common mode ZA BCOMm - Common mode ZB |
<num_x> |
The X-axis position (ns), where the Y-axis value will be returned. |
Examples |
AFR:STANdard:DATA:IMPedance:MARKer:Y? AOP,ADIF,0.5 |
Return Type |
Numeric |
Default |
Not Applicable |
(Read-Write) For the selected fixture, this command reads the fixture length for both 1X or 2X AFR, or sets the fixture length for 1X AFR. Note: After setting fixture length to a new value, the preview command must be sent to apply the value. |
|
Parameters |
|
<char> |
Selected fixture. Choose from: AFIXture - Fixture A. BFIXture - Fixture B. |
<num> |
Fixture length value. Unit is ns. |
Examples |
AFR:STANdard:EDIT:FLENgth
AFIX,0.3273 |
Query Syntax |
AFR:STANdard:EDIT:FLENgth? AFIX |
Return Type |
Numeric |
Default |
Not Applicable |
(Read-Write) This command sets or reads the gate position for the selected fixture. Note: After setting a new gate position, the preview command must be sent to apply the new position. |
|
Parameters |
|
<char> |
Selected fixture. Choose from: AFIXture - Fixture A. BFIXture - Fixture B. |
<num> |
Gate position value. Unit is ns. |
Examples |
AFR:STANdard:EDIT:GATE
AFIX,0.485 |
Query Syntax |
AFR:STANdard:EDIT:GATE? AFIX |
Return Type |
Numeric |
Default |
Not Applicable |
(Write-only) This command sets the impedance for the selected term. |
|
Parameters |
|
<char> |
Impedance term. Choose from: ASENded - Single-Ended ZA. BSENded - Single-Ended ZB. ADIFf - Differential ZA. BDIFf - Differential ZB. ACOMm - Common mode ZA. BCOMm - Common mode ZB. |
<num> |
Impedance value. Unit is Ohms. |
Examples |
AFR:STANdard:EDIT:IMPedance ASEN,52.5 |
Default |
Not Applicable |
(Read-Write) This command sets the impedance method. |
|
Parameters |
|
<char> |
Impedance method. Choose from: DEFault AUTO USER |
Examples |
AFR:STANdard:EDIT:IMPedance:METHod AUTO |
Query Syntax |
AFR:STANdard:EDIT:IMPedance:METHod? |
Return Type |
Character |
Default |
DEFault |
(Read-Write) This command loads the calibration standards data from a file. |
|
Parameters |
|
<char> |
Standards type. Choose from: THRU- 2X Thru. STHRu - Second 2X Thru. FDUT - Fixtured DUT. AOPen - Fixture A Open. BOPen - Fixture B Open. ASHort - Fixture A Short. BSHort - Fixture B Short. |
<string> |
File path of existing measurement data (touchstone 1.0, touchstone 2.0, or citifile). |
Examples |
AFR:STANdard:LOAD AOPen,'C:\open.s1p' |
Query Syntax |
AFR:STANdard:LOAD? AOPen |
Return Type |
String |
Default |
Not Applicable |
(Read-Write) This command specifies fixture thru settings. |
|
Parameters |
|
<char> |
Thru type. Choose from: KNOWn - Known thru, flush thru, or user input length. UNKNown - Unknown thru length computed using reflects. |
<num> |
User input thru length. Default is 0. |
Examples |
AFR:STANdard:THRU KNOW,0 |
Query Syntax |
AFR:STANdard:THRU? |
Return Type |
String |
Default |
"KNOW,0" |
(Read-Write) This command chooses the calibration standards. |
|
Parameters |
|
<char> |
Choose from: THRU- 2X Thru. STHRu - Second 2X Thru. FDUT - Fixtured DUT. AOPen - Fixture A Open. BOPen - Fixture B Open. ASHort - Fixture A Short. BSHort - Fixture B Short. |
<bool> |
Use calibration standards or not. Choose from: ON (or 1) - Use calibration standards. OFF (or 0) - Do not use calibration standards. |
Examples |
AFR:STANdard:USE AOPen,ON |
Query Syntax |
AFR:STANdard:USE? |
Return Type |
String of used standards, separated by commas. For example, use AOPen and BOPen returns: "AOPen,BOPen" |
Default |
All standards - OFF |