SCPI Command Tree


See Also


ABORt

Stops all sweeps

AFR

Automatic Fixture Removal

+ CALCulate    Click to hide and show CALC branches

CORRection

Electrical Delay and Phase Offset

CUSTom

Custom measurements

DATA

Sends and queries data.

DIQ

Differential IQ measurement

EQUation

Equation Editor

FILTer

Time domain gating

FORMat

Display format

FSIMulator

Balanced measurements and Fixturing

FUNCtion

Trace Statistics

GCData

Read Gain compression data

GCMeas

Gain Compression Analysis

GDELay

Group Delay Aperture setting

LIMit

Limit lines for pass / fail testing

MARKer

Marker settings

MATH

Math / Memory

MIXer

X-axis display for FCA measurements

NORMalize

Receiver power cal (Obsolete)

OFFSet

Mag and Phase offset

PARameter

Create and delete measurements

RDATa?

Queries receiver data

SA

Spectrum Analyzer Markers

SMOothing

Point-to-point smoothing

Trace Hold

Trace Hold

TRANsform

Time domain transform

UNCertainty

Uncertainty Trace Properties

X:AXIS

X-Axis Domain

CALPod

Controls CalPod units

CONTrol

Interface control, ECal module state control, and Rear-panel connector control.

CSET

Work with a Cal Set without having to select it into that channel.

DISPlay

Display settings

FORMat

Format for data transfer

HCOPy

Hardcopy printing

INITiate

Continuous or manual triggering

LXI

LXI communications

MMEMory

Saves and recalls instrument states

OUTPut

Turns RF power ON and OFF

ROUTe

Controls internal switch to reference receiver. (Opt 81)

+ SENSe     Click to hide and show SENSe branches

Active (Hot) Parameters

Active Parameters

AVErage

Sweep Averaging

BANDwidth

IF Bandwidth

CLASs

Returns measurement class name

CORRection

Calibration and other correction settings

    | CKIT

Manage Cal Kits and ECal modules

    | COLL:CKIT

Edit Cal Kit definitions

    | COLL:GUIDed

Perform Guided Cals

   | COLL:SESSion

Perform SMC and VMC calibrations

    | CSET

Manage Cal Sets

    | EXTension

Port Extensions

   | IMD

Controls IMD and IMDx calibration

COUPle

Chopped or Alternate sweep

DIQ

Differential IQ

ECAL:CHARacterize

Ecal user characterization

FOM

Frequency Offset (opt 080)

FOM Segment

Construct a segment table

FREQuency

Frequency sweep settings

GCSetup

Gain Compression App (opt 086)

IF

IF Access settings

IMD

Intermodulation Distortion (opt 087)

IMS

Intermodulation Spectrum (opt 087)

MIXer

FCA measurements (opts 082 and 083)

MIXer Embed LO

Allows measurements of mixers with embedded LO

MIXer Segment

Configures mixer segments

MULTiplexer

Controls external test sets

NOISe

Noise Figure (opt 029)

PATH

Provides access to hardware configuration

POWer

Receiver attenuation and overpower protection

PULSe

Configure internal pulse generators

ROLE

Assign sources to roles

ROSCillator

Returns the source of the reference oscillator

SA

Spectrum Analyzer settings

SEGMent

Segment sweep settings

SWEep

Sweep types

SWEep Pulse

Pulse measurements

TEMPerature

Returns the temperature on the receiver board

X:VALues

Returns X-axis values for channel

 

SOURce

Source power to the DUT

    DC

DC Source control

    Multi-Dimensional Sweep

Multi-dimensional sweep control on a Spectrum Analyzer channel

    PHASe

Phase control (Opt 088)

    POWer:CORR

Source power calibration

        ALC:MODE:REC

Receiver Leveling

STATus

Reads the PNA status registers

+ SYSTem    Click to hide and show SYSTem branches

SYSTem

PNA system setting commands

    | CAL:All

Calibrate All Channels

    | CAL:Phase

Perform an SMC Phase Reference Cal

   | CAPability

Reads various capabilities of the analyzer

    | COMMunicate

Controls and queries PNA settings

    | CONF:EDEV

Configure external devices

    | CONF:EDEV:DC

Configures external SMU, DC Meter, and DC Source properties

   | CONF:EDEV:PMAR

Configures external Power Meter as Receiver

    | CONF:MWAVe

Configure Millimeter Wave measurements

    | CORR:INTerpolate:LINear

Linear interpolation

    | FIFO

Controls data in and out of FIFO data buffer

    | PREFerences

VNA Preferences

    | UNCertainty

Dynamic Uncertainty

TRIGger

Trigger measurements