|
(Read-Write) Throws internal switch to reference receiver when the specified channel is measured. N523xA models do NOT have the R1 reference receiver switch. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1 |
|
<char> |
Position of the switch. Choose from: INTernal - bypass R1 Loop. Connects the port 1 source directly to the R1 receiver. EXTernal - flow through R1 Loop. Allows direct access to the R1 receiver through the Reference 1 front-panel connectors. |
|
Examples |
ROUT:PATH:LOOP INT |
|
Query Syntax |
ROUTe<cnum>:PATH:LOOP:R1? |
|
Return Type |
Character |
|
INTernal |
|