|
Replaced with CALC:X? (Read-only) Returns the stimulus values for the specified channel. If the channel is sweeping the source backwards, the values will be in descending order. Note: To avoid frequency rounding errors, specify FORM:DATA <Real,64> or <ASCii, 0> |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
Examples |
SENS:X? |
|
Return Type |
Depends on FORM:DATA command |
|
Not applicable |
|
Last Modified:
|
16-Aug-2013 |
Superseded per JE |
|
10-Sep-2012 |
Added Form:Data note |
|
9-Apr-2010 |
Added Note |