This VB Script program configures a new Power Meter as Receiver device and creates a trace using the PMAR.
Learn more about Power Meter as a Recevier
These programs can be run as a macro in the PNA. To do this, copy the code into a text editor file such as Notepad and save on the PNA hard drive as PMAR.vbs. Learn how to setup and run the macro.
See all External Device Configuration commands
See Other SCPI Example Programs
|
' This section gets the PNA application ' starts the scpi parser, and presets the PNA dim app Set app = CreateObject("AgilentPNA835x.Application") set scpi = app.ScpiStringParser scpi.parse "*rst" scpi.parse "Syst:conf:edev:add 'newpmar1'" scpi.parse "Syst:conf:edev:dtype 'newpmar1', 'Power Meter'" scpi.parse "Syst:conf:edev:driver 'pmar', 'AGPM'" scpi.parse "Syst:conf:edev:ioconfig 'newpmar1', 'gpib0::14::instr'" scpi.parse "Syst:conf:edev:pmar:sens 'newpmar1', 1" scpi.parse "Syst:conf:edev:pmar:read:count 'newpmar1', 10" scpi.parse "Syst:conf:edev:pmar:read:ntolerance 'newpmar1', 0.1" scpi.parse "Syst:conf:edev:pmar:sens 'newpmar1', 1" scpi.parse "Syst:conf:edev:pmar:fmin 'newpmar1', 100000000" scpi.parse "Syst:conf:edev:pmar:fmax 'newpmar1', 10000000000" scpi.parse "Syst:conf:edev:pmar:flim 'newpmar1', 0" scpi.parse "Syst:conf:edev:pmar:tabl:rfac 'newpmar1', 100" scpi.parse "Syst:conf:edev:pmar:tabl:cfac:freq 'newpmar1', 1e9, 2e9, 3e9" scpi.parse "Syst:conf:edev:pmar:tabl:cfac:data 'newpmar1', 99, 98, 99" scpi.parse "Syst:conf:edev:pmar:tabl:loss:stat 'newpmar1', 1" scpi.parse "Syst:conf:edev:pmar:tabl:loss:freq 'newpmar1', 1e9, 2e9, 3e9" scpi.parse "Syst:conf:edev:pmar:tabl:loss:data 'newpmar1', -1, -2, -3" 'Activate and enable the PMAR external device scpi.parse "Syst:conf:edev:ioen 'newpmar1', 1" scpi.parse "Syst:conf:edev:stat 'newpmar1', 1" 'Create a PMAR trace with power meter connected to port 3 'Use Calc:Par:Def:Ext - NOT CALC:PAR:DEF!! scpi.parse "CALC:PAR:DEF:EXT 'myPMARTrace', 'newpmar1,3'"
|
Last Modified:
|
11-Feb-2011 |
Renamed |
|
3-Sep-2009 |
MX New topic |