This VB Script program configures an External Source.
Learn more about External Source Configuration
These programs can be run as a macro in the PNA. To do this, copy the code into a text editor file such as Notepad and save on the PNA hard drive as ExtSource.vbs. Learn how to setup and run the macro.
See all External Device Configuration commands
See Other SCPI Example Programs
|
' Get the PNA application, and ' start the scpi parser, and preset the PNA dim app Set app = CreateObject("AgilentPNA835x.Application") set scpi = app.ScpiStringParser scpi.parse "*rst" ‘Configure the external source scpi.parse "Syst:conf:edev:add 'newSource'" scpi.parse "Syst:conf:edev:dtype 'newSource', 'Source'" scpi.parse "Syst:conf:edev:driver 'newSource', 'AGMXG'" scpi.parse "Syst:conf:edev:ioconfig 'newSource', 'gpib0::16::instr'" 'Activate and enable the external source scpi.parse "Syst:conf:edev:ioen 'newSource', 1" 'State activates and talks to the device if "Syst:conf:edev:ioen" is enabled scpi.parse "Syst:conf:edev:stat 'newSource', 1"
|
Last Modified:
|
7-Sep-2011 |
Minor edit |
|
11-Feb-2011 |
New topic |