This program configures several Swept IMDx parameters using power sweep. In this configuration, tone power is swept from -20 dBm to -5 dBm while the Input, LO, and Output frequencies are fixed as follows:
Input center freq= 2.50 GHz
Tone Delta freq = 10 MHz (f1 = 2.495 GHz and f2 = 2.505 GHz).
LO freq = 2.00 GHz
Output freq = 4.50 GHz
This program also allows you to optionally load a .mxr file to perform mixer setup.
To run this program without error, an external source named 'PSG' must be connected to drive the LO.
This program can be run as a macro in the PNA. To do this, copy the code into a text editor file such as Notepad and save on the PNA hard drive as IMDX.vbs. Learn how to setup and run the macro.
See Other SCPI Example Programs
|
Dim app Dim scpi Dim err ' 'Create / Get the PNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser ' 'Preset the system scpi.parse "SYST:FPR" scpi.parse "DISP:WIND1:STAT ON" ' 'Create an IMDX measurement in Channel 1 and display it as trace 1 in window 1 scpi.parse "CALC1:CUST:DEF 'ch1IMDX', 'Swept IMD Converters', 'PwrMain'" scpi.parse "DISP:WIND1:TRAC1:FEED 'ch1IMDX'" ' 'Put the channel in trigger hold scpi.parse "SENS:SWE:MODE HOLD" scpi.parse "SENS:IMD:SWE:TYPE POW" 'Put the channel in trigger hold and setup all the mixer parameters scpi.parse "SENS1:SWE:MODE HOLD" scpi.parse "SENS1:IMD:SWE:TYPE POW" scpi.parse "SENS1:MIX:INP:FREQ:MODE FIXED" scpi.parse "SENS1:MIX:LO:FREQ:MODE FIXED" scpi.parse "SENS1:MIX:OUTP:FREQ:MODE FIXED" scpi.parse "SENS1:MIX:INP:FREQ:FIX 2500000000" scpi.parse "SENS1:MIX:LO:FREQ:FIX 2000000000" scpi.parse "SENS1:MIX:OUTP:FREQ:SID HIGH" scpi.parse "SENS1:MIX:CALC OUTP" scpi.Parse "SENS:MIX:APPLY" 'First apply the settings, then set LO Name scpi.Parse "SENS:MIX:LO:NAME 'PSG'" scpi.parse "SENS1:MIX:LO:POW 10" scpi.Parse "SENS:MIX:APPLY"
'Optionally, put the channel in hold and load an 'existing .mxr file with all the mixer settings 'scpi.parse "SENS1:SWE:MODE HOLD" 'scpi.parse "SENS1:MIX:LOAD 'c:\users\public\network analyzer\documents/Mixer/IMD/Ch1.mxr'" ' 'Make additional IMD settings scpi.parse "SENS1:IMD:TPOW:COUP:STAT ON" scpi.parse "SENS1:IMD:TPOW:F1:STAR -20" scpi.parse "SENS1:IMD:TPOW:F1:STOP -5" scpi.parse "SENS1:IMD:FREQ:DFR:CW 10000000" scpi.parse "SENS1:SWE:POIN 201" scpi.parse "SENS1:imd:ifbw:main 1000" scpi.parse "SENS1:imd:ifbw:imt 500" scpi.parse "SOUR1:POW2:AMPL -5" ' 'Create additional measurements in the channel scpi.parse "CALC1:CUST:DEF 'ch1IMDX2', 'Swept IMD Converters', 'IM3'" scpi.parse "DISP:WIND1:TRAC2:FEED 'ch1IMDX2'" scpi.parse "CALC1:CUST:DEF 'ch1IMDX3', 'Swept IMD Converters', 'OIP3'" scpi.parse "DISP:WIND1:TRAC3:FEED 'ch1IMDX3'" scpi.parse "CALC1:CUST:DEF 'ch1IMDX4', 'Swept IMD Converters', 'IIP3'" scpi.parse "DISP:WIND1:TRAC4:FEED 'ch1IMDX4'" scpi.parse "CALC1:CUST:DEF 'ch1IMDX5', 'Swept IMD Converters', 'ToneGain'" scpi.parse "DISP:WIND1:TRAC5:FEED 'ch1IMDX5'" ' 'Take a single sweep to apply all stimulus changes scpi.parse "*cls;*ese 1" scpi.parse "sens1:swe:mode SING;*OPC?" ' 'Check for errors err=scpi.parse ("SYST:ERR?") MsgBox(err) |
Last Modified:
|
8-Mar-2012 |
Updated LO name order (ZW) |
|
21-Sep-2010 |
Fixed error |
|
15-Jul-2010 |
MX New topic |