This example allows you to calibrate multiple SMC channels while connecting the power meter and required standards or ECal module only once.
In the example program:
Modify chans = 2 to indicate the number of channels to calibrate.
You can also change the connector type and cal kit for each port.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as MultChanCal.vbs. Learn how to setup and run the macro.
|
Dim app Dim scpi Dim chans Dim i Dim steps Dim desc ' Create / Get the PNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser app.Preset ' Set number of channels to create chans = 2 ReDim calset(chans - 1) For i = 1 To chans chanStr = CStr(i+1) ' calibrate on channels 2 and 3 Dim parm, measName, sens, calc parm = "S" & CStr(i) & CStr(i) measName = "My" & parm sens = "SENS" & chanStr calc = "CALC" & chanStr scpi.Parse calc & ":CUST:DEF '" & measName & "', 'Scalar Mixer/Converter', '" & parm & "'"
'Setup the new measurement as the 2nd trace in the active window scpi.Parse "DISP:WIND:TRAC" & chanStr & ":FEED '" & measName & "'" 'Make the new trace the active measurement scpi.Parse calc & ":PAR:SEL '" & measName & "'"
'--------------Perform A FCA Mixer Calibration------------- 'Set ports and cal kits for 2 port calibration portion scpi.Parse sens & ":CORR:COLL:GUID:CONN:PORT1:SEL ""APC 3.5 male""" scpi.Parse sens & ":CORR:COLL:GUID:CONN:PORT2:SEL ""APC 3.5 female""" scpi.Parse sens & ":CORR:COLL:GUID:CKIT:PORT1:SEL ""85052C""" scpi.Parse sens & ":CORR:COLL:GUID:CKIT:PORT2:SEL ""85052C""" 'ECal modules are specified with the same command ' scpi.Parse sens & ":CORR:COLL:GUID:CKIT:PORT1:SEL ""N4691-60004 ECal""" ' scpi.Parse sens & ":CORR:COLL:GUID:CKIT:PORT2:SEL ""N4691-60004 ECal"""
'Specify the thru measurement method. scpi.Parse sens & ":CORR:COLL:GUID:PATH:TMET 1,2,""DEFINED THRU"""
'Omit the isolation part of the 2-port cal scpi.Parse sens & ":CORR:COLL:GUID:ISOL NONE"
'Initialize an SMC guided calibration. scpi.Parse sens & ":CORR:COLL:GUID:INIT" 'Determine the number of steps required to complete the calibration. steps = scpi.Parse (sens & ":CORR:COLL:GUID:STEP?") Next For j = 1 To CInt(steps) 'Display the prompt for each step desc = scpi.Parse(sens & ":CORR:COLL:GUID:DESC? " & CStr(j)) MsgBox (desc) 'Measure the same standard for each channel For i = 1 To chans chanStr = CStr(i+1) ' channel number as string scpi.Parse "SENS" & chanStr & ":CORR:COLL:GUID:ACQ STAN" & CStr(j) opc_comp = scpi.Parse("*OPC?") Next Next 'Finish the cal and save the calsets For i = 1 To chans calset(i - 1) = scpi.Parse("SENS" & CStr(i+1) & ":CORR:COLL:GUID:SAVE ON") Next MsgBox ("SMC Cals Complete!")
|
Last Modified:
|
15-Mar-2011 |
Modified for FCA2 |
|
6-Feb-2008 |
MX New topic |