This example program creates a Noise Figure measurement, then calibrates the measurement.
You MUST change the ECal Identification strings (in Blue font).
Optional: Uncomment the following lines (in Blue font) to change these settings:
Noise Receiver = Noise Receiver to Std (PNA) Receiver
Cal Method = "Vector" to "Scalar"
Receiver Characterization Method = "NoiseSource" to "PowerMeter"
This VBScript program can be run as a macro in the PNA. To do this, copy the code into a text editor file such as Notepad and save on the PNA hard drive as NF.vbs. Learn how to setup and run the macro.
See the Noise figure commands.
See Other SCPI Example Programs
|
' This section gets the PNA application ' starts the scpi parser, and presets the PNA windowNum = 1 channelNum = 1 set pna=CreateObject("AgilentPNA835x.Application") set scpi = pna.ScpiStringParser ' Create noise figure measurement scpi.Parse "SYST:FPR" scpi.Parse "DISP:WIND ON" scpi.Parse "CALC:CUST:DEF 'noiseFig', 'Noise Figure Cold Source', 'NF'" scpi.Parse "DISP:WIND:TRAC:FEED 'noiseFig'" scpi.Parse "CALC:PAR:SEL 'noiseFig'" ' Substitute appropriate Ecal identification strings here tunerEcal = "N4691-60004 ECal 02821" pullEcal = "N4691-60004 ECal 02297" ' configure channel ConfigureChannel ConfigureNoiseSettings ' perform calibration SetupNoiseSource SetupCalAttributes_Insertable FinishCalibration ' ----- Support subroutines ------ ' Configure noise channel sub ConfigureChannel scpi.Parse "SENS:FREQ:START 750MHz" scpi.Parse "SENS:FREQ:STOP 5.0GHz" scpi.Parse "SENS:SWEEP:POINTS 401" scpi.Parse "SENS:BWID 1.0E3" end sub ' Configure noise-specific channel settings sub ConfigureNoiseSettings scpi.Parse "SENS:NOIS:REC NOISe" 'Use noise receivers ' scpi.Parse "SENS:NOIS:REC NORM" 'Use std PNA receiver scpi.Parse "SENS:NOIS:AVER:STAT ON" ' turn averaging ON scpi.Parse "SENS:NOIS:AVER 40" ' noise averaging scpi.Parse "SENS:NOIS:BWID 8MHz" ' noise bandwidth scpi.Parse "SENS:NOIS:GAIN 30" ' gain of noise receiver scpi.Parse "SENS:NOIS:TEMP:AMB 301" ' ambient temperature, in Kelvin scpi.Parse "SENS:NOIS:IMP:COUN 5" ' number of tuner impedance states scpi.Parse "SENS:NOIS:TUN:ID '" & tunerEcal & "'" ' set ID of tuner Ecal module scpi.Parse "SENS:NOIS:TUN:INP 'B'" ' orientation of tuner input port scpi.Parse "SENS:NOIS:TUN:OUTP 'A'" ' orientation of tuner output port scpi.Parse "SENS:CORR:TCOL:USER:VAL 300" ' noise source cold temperature end sub
sub SetupCalAttributes_Insertable scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT1 'APC 3.5 female'" scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT2 'APC 3.5 male'" scpi.Parse "SENS:CORR:COLL:GUID:CKIT:PORT1 '" & pullEcal & "'" ' port 1 calkit scpi.Parse "SENS:CORR:COLL:GUID:CKIT:PORT2 '" & pullEcal & "'" ' port 2 calkit
scpi.Parse "SENS:NOIS:SOUR:CONN 'APC 3.5 male'" ' noise source connector type scpi.Parse "SENS:NOIS:SOUR:CKIT '" & pullEcal & "'" ' noise source calkit scpi.Parse "SENS:NOISe:CAL:METHOD 'Vector'" ' cal method ' scpi.Parse "SENS:NOISE:CAL:METHOD 'Scalar'" scpi.Parse "SENS:NOISE:CAL:RMEThod 'NoiseSource'" 'Receiver Characterization method ' scpi.Parse "SENS:NOISE:CAL:RMEThod 'PowerMeter'" scpi.Parse "SENS:CORR:COLL:GUID:INIT" end sub
sub SetupNoiseSource ' specify the ENR file for the noise source enrfile = "C:/Program Files/Keysight/Network Analyzer/Noise/346C_MY44420454.enr" scpi.Parse "SENS:NOIS:ENR:FILENAME '" & enrfile & "'" ' set noise source cold temperature scpi.Parse "SENS:CORR:TCOLd:USER:VAL 301.1" end sub
sub FinishCalibration ' Build the connection list and acquire the calibration steps = scpi.Parse("SENS:CORR:COLL:GUID:STEPS?") for i = 1 to steps str = scpi.Parse("SENS:CORR:COLL:GUID:DESC? " & i) msgbox str scpi.Parse "SENS:CORR:COLL:GUID:ACQ STAN" & i next scpi.Parse "SENS:CORR:COLL:GUID:SAVE 0" wscript.echo "Calibration complete" end sub |
Last Modified:
|
9-Jun-2011 |
Updated with Rcvr Char Method A.09.41. |