|
|
This 15-pin female D-sub connector allows connection of external VGA monitors. With the following resolution settings, you can simultaneously view the PNA display and a remote monitor. |
||||||||
|
|||||||||
|
2. Right-click on the PNA desktop, then click Properties |
|
3. Click the Settings tab |
|
4. Click Advanced |
|
5. Click Intel(R) Extreme...tab. |
|
6. Click Graphics Properties button. |
|
7. Under Multiple Display, click Intel(R) Dual Display Clone. |
|
8. Click OK, then OK again to confirm. |
The PNA must be set to the default resolution (640 x 480). While on any other resolution setting, only the external monitor can be viewed. To change resolution:
Right-click on the PNA desktop, then click Properties.
Click the Settings tab.
Adjust display resolution.
Repeat above "turn ON" procedure except for following:
6. Under Single Display, click Notepad
Last modified:
|
11-Apr-2012 |
Removed old content |