Drive mapping allows you to share disk drives between the PNA and an external computer.
Both the PC and PNA must be connected to a shared computer network
You must know the full computer name of the Analyzer you are mapping TO. Tell me how
Note: This procedure requires a mouse and keyboard.
Map to a drive on the PNA from an External PC
On the analyzer desktop, click Windows Explorer. Right-click on the drive you want to share. Click Sharing...
In the dialog box, select Shared this folder. In the Share Name box, type in a share name for the drive. For example: C$. Click OK.
On the external PC desktop, click Windows Explorer. From the Tools menu, click Map Network Drive.
If the current logon on your PC is different from the current logon on the analyzer, click Connect using a different Logon to connect to using the current analyzer logon, .This logon must be registered on the external PC. To see the current logon on either the PC or analyzer, hold Ctrl - Alt, and press Delete.
In the Connect as box, type the logon currently being used by the analyzer.
In the Password box, type the logon password that you use on the external computer. Click OK
In the Folder box, type //computername (prep1)/share name (from step 2). (For example: //SLT1234/C$ )
Click Finish.
Last Modified:
|
25-Nov-2013 |
Modified for Win7 |