The cables and adapters listed in the dialog box.
Note: You must be logged onto the PNA as an Administrator to perform an adjustment. Learn more.
Click Utilities, then System, then Service, then Adjustments
At the Adjustments selection, clickReceiver Characterization
Follow prompts in the program.

Select the receivers to be characterized, or click Select All.
The correction data is stored in the flash memory on the Test Set Mother Board.
Last Modified:
|
3-Jan-2014 |
Updated |
|
20-Jan-2007 |
MX New topic |