This feature allows you to read the current temperature on the receiver microcircuit.
This feature is available on ALL models except the N523x models and the 4-port N5244A and N5245A models with DSP Version 4.
To read temperature, press System, then Service, then Utilities, then Receiver Temperature.
The temperature reading is updated with every sweep.
Temperature is available in Celsius and Fahrenheit.
Temperature can also be read using remote commands.
SCPI: SENSe:TEMPerature?
COM: ReceiverTemperature