Click Help, then About Network Analyzer to learn the capabilities of your analyzer.

Model number (see list of PNA models)
Frequency range
Serial number
Options (Learn how to install software options)
Application Code (firmware) Version
Hard Disk Drive Version
System CPU Version - Learn more
DSP (Digital Signal Processor.) Version. Contact Keysight to upgrade the DSP. See DSP Version changes below.
Computer Name - Learn more. This is also reported on the LAN Status / LXI Compliance dialog.
For PNA-X, the DSP board number along with the FPGA version, provides access to the following features or causes the following settings to change:
|
DSP Board |
FPGA Version |
Changes |
|
4 |
27 |
Enabled FastCW triggering |
|
4 |
34 |
Enabled configurable (polarity and type) for PulseSyncIn external trigger signals. |
|
5 |
xx* |
IF Frequencies – The default values are changed. IFAntiAliasFilter - The Narrow and Wide settings are changed. Note: Programs that control the following DSP filter settings, or state files that are saved with these settings, will yield different results when run or recalled on PNAs with DSP 4 versions versus DSP 5 versions.
|
*With DSP board 5, FPGA version is upgraded with firmware. This requires more time for FW installation.