Using Data and Memory

Other topics about Making Measurement

Data displayed on the graph plot can be stored in the memory and recalled for later use. Data traces stored in the memory will be deleted once TDR option restarts.

Storing Data Traces to Memory

  1. Click on the Data Mem button.

  2. Select Data -> Mem from the list.

Display the Memory Traces

  1. Click on the Data Mem button.

  2. Select Memory from the list.

Table below explains other functions in the Data Mem list:

Function

Details

Data -> Mem

Save Data traces to Memory

Off

Display off

Data

Display Data traces only

Memory

Display Memory traces only

Data & Memory

Display Data and Memory traces