DPD Overview

The Digital Predistortion (DPD) feature in the VNA characterizes and then creates a model of the non-linear distortions of power amplifiers caused when operating in the amplifier's compression region. DPD then creates a DPD waveform (inverse distortion) so that the DUT output will approximate the desired ideal waveform. DPD provides improved linearity to allow transmission of signals at lower distortion levels.

Note: Digital Predistortion is a Licensed Feature. Learn more about Licensed Features.

In this topic:

See Also

Features and Requirements

Features

Requirements

DPD Waveforms

The diagram shows the signal flow and waveforms through the VNA to the DUT input and output.

Waveform

Description

Ideal

This is the desired Ideal waveform, which is the default modulation file currently selected in the Modulate tab of the Modulation Distortion Setup dialog.

Ideal DPD

The model is applied to the Ideal waveform to create the Ideal DPD waveform. This waveform does not have source correction applied.

Corrected DPD

Ideal DPD waveform with source correction applied.

~Ideal DPD

DUT input signal with DPD and source correction applied. This approximates the Ideal DPD waveform.

~Ideal

The DUT output signal with DPD and source correction applied. This approximates the Ideal waveform. Most of the distortion from the DUT is tuned out of the signal at this point.

The following example shows a typical Ideal Waveform and DUT Output without DPD applied.

After applying DPD, the following shows typical ~Ideal DPD and ~Ideal waveforms.

DPD File Structure

The following table describes the files in the DPD file structure:

Filename

File Description

MyDPD_Ideal.csv

This is the original Ideal Waveform.

MyDPD_IdealDPD.csv

Ideal DPD waveform without source correction applied.

MyDPD_CorrDPD.csv

Ideal DPD waveform with source correction applied.

DUTIn.csv

Waveform measured at the DUT input which is used to create the DPD Model.

DUTOut.csv

Waveform measured at the DUT output which is used to create the DPD Model.

DUTLinearGain.csv

Contains the linear gain of the DUT if the DPD model is Dynamic Gain.

mod.manifest

File containing setup information.

DPDModel.csv

Contains the DPD model parameters.

Direct DPD

Direct DPD determines the maximum possible improvement to in-band EVM. This method generates a predistorted signal and does not use a model.

Modeled DPD

The following diagram shows the measurement flow for modeling.

Memory Polynomial Modeling

Memory Polynomial Modeling is a technique that uses a memory polynomial algorithm to create the model. This model depends on past and future input values to account for memory effects. The past/future input values define the number of input past/future time samples to use for calculating the current output sample.

Dynamic Gain Modeling

Note: Dynamic Gain of measurements above 50 GHz requires the S93110B Active Hot Parameters license

Dynamic Gain Modelling is a technique that uses dynamic gain algorithm to create the model. The gain is characterized by the AM-AM (magnitude ) and AM-PM ( phase) functions, which are associated with the memory operators. There are a total of four memory operators that users can choose from to include in the gain algorithm.