There are many reasons to configure the front-panel jumpers on the VNA.
Note: Phase-locking and the Reference Receivers The R1 and R2 reference receivers are used for phase-locking between the RF source and receiver LO. The phase-locking requirement imposes the following restrictions on the reference signal:
In Frequency Offset Mode (FOM) Opt S93080A, the R1 receiver is NOT used for phase locking. Independent internal circuitry is used to phase lock the source and receivers. When FOM is available, turn FOM ON simply to take advantage of the independent phase locking mechanism. If NOT measuring at different source and receiver frequencies, set the offset to zero, so that the source and receiver frequencies are the same. |