mmWave Measurements without a Test Set


This topic describes the basic configuration needed to connect a waveguide transmission reflection frequency extender directly to a PNA-X (without a N526x test set). This configuration will allow you to create an integrated 2-port banded waveguide S-Parameter measurement solution. In particular, it will focus on the options and configurations of the PNA-X as well as the settings required to make a complete measurement.

See Also

mmWave Configuration with a N526x Test Set

Requirements

Limitations

Hardware Connections

The following list of components applies to the example shown above:

Connect the frequency extenders to the VNA as shown below:

Legend

Remove the jumper cables, then connect to the Receiver IN connectors.

Color

VNA to 1st Module

(VNA to 2nd Module)

mmWave Module

Orange

Rcvr Ref 1 IN

(Rcvr Ref 2 IN)

Ref IF Out

Blue

Rcvr A IN

(Rcvr B IN)

Test IF Out

Red

Port 1

(Port 2)

RF In

Green

Port 3

(Port 4)

LO In

VNA Settings

Note: A macro is available that makes the following VNA settings automatically. Learn more.

  1. In Power and Attenuators dialog:

    1. Set the Port 3 and Port 4 power to ON. (This allows LO power to always be ON).

    2. Adjust the port power to adequately drive the mmWave module (12 dBm is this example).

    3. Clear the Port Powers Coupled checkbox if the LO and RF power requirements are different.

  2. In Path Configuration dialog, Set Port 1 Ref Switch to External.  This is NOT necessary for rear-panel connections and on a second mmWave module connected to ports 2 and 4.

  3. In FOM dialog:

Note: The following procedure shows mmWave frequencies from 75 GHz to 110 GHz.

To make the following Multiplier, Divisor, and Frequency settings, click in the Settings field for the corresponding Source or Receiver, then click Edit.

    1. Source (RF): Set Divisor to 6.
    2. Receivers: Set Offset to 100 MHz and Multiplier to 0.
    3. Source 2 (LO): Set Offset to 12.5 MHz and Divisor to 8.
    4. Set all modes to Coupled.
    5. Check Frequency Offset: ON
    6. Set Primary: Start 75 GHz - Stop 110 GHz
    7. Set X-Axis Display Annotation to Primary.

4. In Calibration Preferences dialog: To calibrate at the mmWave frequencies check the Use FOM Primary Frequency.

Using the Macro

Using the macro will eliminate all of the steps involved in setting up the power and the attenuators as well as the Frequency settings.

Load the macro and enter the values for setting up the measurement.