This example performs a user-characterization and stores it to both the ECal module memory and VNA disk memory.
It then performs two 2-port cals: the first using the characterization from module memory, then using the characterization from disk memory.
Note: This example requires that channel 1 be already calibrated.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file, such as Notepad, and save it on the VNA hard drive as ECal.vbs.
How to setup and run the macro.
See Other COM Example Programs
Option Explicit Dim pna Set pna = CreateObject("AgilentPNA835x.Application") Dim calMgr Set calMgr = pna.GetCalManager ' Get ECal User Characterizer COM object Dim ecalCharacterizer Set ecalCharacterizer = calMgr.GetECalUserCharacterizer ' Substitute here the model number and serial number of your own ECal. ' Note that this example corresponds to a 4-port ECal module with ' serial number 00001. If instead you have a 2-port ECal module, ' their model numbers are '5x5' numbers -- for example, 'N4691-60001'. Dim ecalModelNum ecalModelNum = "N4433A" Dim ecalSerialNum ecalSerialNum = "00001" ecalCharacterizer.ECalID = ecalModelNum & "," & ecalSerialNum MsgBox "ECal module to be characterized is: " & ecalCharacterizer.ECalID ' Set which user characterization number (1-12) the new characterization ' will be stored to in the ECal module when it is done. If you intend to ' store your user characterization just to VNA Disk Memory and NOT the ' ECal module's memory, then omit the setting of this property. ecalCharacterizer.CharacterizationNumber = 1 ' The following commented-out lines of code show how you can access ' the list of connector type names you can set for the ports of an ' ECal when you user-characterize it. However, please note that if ' you are writing the user characterization to the ECal module's memory, ' as of yet only the Factory Defined set of connector choices will work ' properly (see the ValidConnectorType property). ' If you will be saving your characterization to just ' VNA Disk Memory only, then all connector names returned by this call ' will work, user-defined connector names as well as factory-defined. 'Dim connTypeArray 'connTypeArray = ecalCharacterizer.ValidConnectorTypes 'MsgBox connTypeArray(1) ' Access element 1 in the string array ' For each port of the ECal module, specify which connector type ' is at the end of the adapter (or cable or fixture) that is ' connected to that port of the ECal for the characterization ' (must be one of the connector types that is included in the ' list that the ValidConnectorTypes method returns). The default ' is "No adapter", which assumes you are characterizing that port ' of the ECal "as is" (nothing attached to it). So in this example, ' Ports C and D of the ECal are being characterized to just the ' ECal's connectors. ecalCharacterizer.ConnectorType(1) = "APC 3.5 male" ' ECal Port A ecalCharacterizer.ConnectorType(2) = "APC 3.5 male" ' ECal Port B ' As with the connector types, the information set in these next ' few properties also gets stored within the characterization. ' Set the name of the person and/or company that is producing ' this characterization. ecalCharacterizer.UserName = "John Doe, Acme Inc." ' Set user-specified description of the VNA being used. ecalCharacterizer.UserDescriptionOfPNA = "SN US12345678" ' Set descriptions of what you have connected to the ECal module's ' ports for the characterization. ecalCharacterizer.PortDescription(1) = "3.5 mm adapter, SN 00001" ' Port A of the ECal ecalCharacterizer.PortDescription(2) = "3.5 mm adapter, SN 00002" ' Port B of the ECal ' Begin a user characterization on Channel 1. ' If you will be storing this characterization to the ECal module's memory, then ' the boolean argument to this command should be set to True. If you will be storing ' this characterization to VNA disk memory ONLY, then you should specify False for ' that argument. In this example we will be storing the characterization to both ' module memory and VNA disk memory, so we use True. ecalCharacterizer.InitializeEx 1, True ' Generate the measurement steps for the user characterization. Dim numSteps numSteps = ecalCharacterizer.GenerateSteps ' Measure the steps. ' You must ensure you have already applied the appropriate calibration to the channel ' already, or else an error will be thrown indicating that. Dim i For i = 1 To numSteps MsgBox ecalCharacterizer.GetStepDescription(i) ecalCharacterizer.AcquireStep(i) MsgBox "Acquire is complete" Next MsgBox "Now the user characterization will be saved to the ECal module and to PNA disk memory" ' Save the user characterization to the ECal module's memory. ' Note that this can take multiple minutes, depending on how ' many sweep points the channel has. ecalCharacterizer.SaveToECal ' Save the user characterization to VNA Disk Memory. Dim characterizationName characterizationName = "test" ecalCharacterizer.SaveToDiskMemory(characterizationName) MsgBox "User characterization is complete. Now we will calibrate using it. First we will use it from ECal module memory." Dim moduleMemCalKitName moduleMemCalKitName = GetCalKitName("User " & CStr(ecalCharacterizer.CharacterizationNumber)) DoTwoPortCal moduleMemCalKitName MsgBox "Now we will calibrate using the characterization from PNA Disk Memory." Dim pnaDiskMemCalKitName pnaDiskMemCalKitName = GetCalKitName(characterizationName) DoTwoPortCal pnaDiskMemCalKitName MsgBox "Example has completed"
Function GetCalKitName(characterizationName) Dim calKitName calKitName = ecalModelNum If Len(characterizationName) > 0 Then calKitName = calKitName & " " & characterizationName calKitName = calKitName & " ECal " & ecalSerialNum GetCalKitName = calKitName End Function
Sub DoTwoPortCal(calKitName) ' Initialize guided cal to be performed on Channel 1. Dim guidedCal Set guidedCal = calMgr.GuidedCalibration guidedCal.Initialize 1, True ' Specify the DUT connector for each VNA port to be calibrated (DUT connector = ECal characterization's connector) guidedCal.ConnectorType(1) = "APC 3.5 male" guidedCal.ConnectorType(2) = "APC 3.5 male" ' Specify the "cal kit" for each of those ports guidedCal.CalKitType(1) = calKitName guidedCal.CalKitType(2) = calKitName ' We know this example will result in a calibration sequence of a single "connection step" Dim numSteps numSteps = guidedCal.GenerateSteps ' Acquire the cal connection step guidedCal.AcquireStep 1 ' Conclude the cal and turn it on guidedCal.GenerateErrorTerms End Sub |