Write-only
 

AcquireStep Method


Description

Acquire the measurement data for the specified step in the calibration process. For an ECal User characterization this measures the ECal module.

Note: Guided Cal allows you to measure standards in any order. See an example.

 VB Syntax

obj.AcquireStep (n)

Variable

(Type) - Description

obj

Any of the following:

GuidedCalibration (object)

SMCType (object)

VMCType (object)

ECalUserCharacterizer (object) - Currently, only ONE step is required to measure the ECal module.

n

 

Step number in the calibration process.

Use GenerateSteps to determine the total number of steps.

Use GetStepDescription to read the description of each step.

Return Type

Not Applicable

Default

Not Applicable

Examples

VMC.AcquireStep (3)

C++ Syntax

HRESULT put_AcquireStep(long step);

Interface

SMCType

VMCType

IGuidedCalibration

IECalUserCharacterizer