Write-only
About Mixer/Converter Settings

AddSegment Method


Description

Adds the specified number of segments to the scratch mixer at the index position.  All segments are added with default settings.

 VB Syntax

conv.AddSegment index,count

Variable

(Type) - Description

conv

A Converter Object

index

(Long integer) Position at which to add segments. Valid index range is between 1 and the current segment count +1. Using count +1 adds segments to the end of the segment table. Use SegmentCount Property to read the current count in the Applied Mixer.

count

(Long integer) Optional argument. Number of segments to add. If unspecified, 1 segment is added.

Return Type

Not Applicable

Default

Not Applicable

Examples

mxr.AddSegment 1,5 'Adds 5 segments beginning at the first position.

See example program

C++ Syntax

HRESULT AddSegment(long index, long count);

Interface

IConverter5