Write-only
About Multiple Power Sensors

Add (GuidedPowerSensors) Method


Description

Adds a power sensor name and item number to be used during a source power calibration. Use when multiple power sensors are to be used to calibrate the entire frequency span. The Name is used to recognize the sensor in the User Interface.

Item numbers in the GuidedCalibrationPowerSensors collection are used to refer to the power sensor remotely.  Use the Count Property to return the number of power sensor items that are configured for use on the channel.

The port number to be calibrated is set using the PerformPowerCalibration Property.

Learn about using multiple power sensors

VB Syntax

sensors.Add (name)

Variable

(Type) - Description

sensors

A GuidedCalibrationPowerSensors (collection)

name

(String) - Name of the power sensor to add. The power sensor must be already configured as a PMAR device using this name. Learn how to remotely configure a PMAR device.

Return Type

Not Applicable

Default

Not Applicable

Examples

sensors.Add "pmar2"

See Example program

C++ Syntax

HRESULT Add(BSTR name);

Interface

IGuidedCalibrationPowerSensors