Write-only |
About External Testset Control |
Description |
Adds a testset to the ExternalTestsets Collection and loads the configuration file. |
VB Syntax |
testsets.Add (model,address) |
Variable |
(Type) - Description |
testsets |
An ExternalTestsets (collection) |
model |
(String) Model of the testset to be added, NOT case-sensitive. There is no COM command to read a list of currently-supported test sets. However, the following SCPI command can be used with the following format: string = SCPISTringParser.Execute ("SENSe:MULTiplexer:CATalog?") |
address |
(Integer) Address of the testset to be added. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
testsets.Add("Z5623AK66",12) ' add Z5623AK66 test at address 12 to testsets collection |
C++ Syntax |
HRESULT Add(BSTR typename, long address) |
Interface |